Para usted

Clippers derrotan a Rockets 113-102 en 5ta…

NBA: Clippers 113, Rockets 102; Lou Williams anota 31 puntos, Blake Griffin añade 29 antes de su expulsión

Multiple Arrests After Brawl Breaks Out at Martin…

At least eight people were arrested after a brawl broke out following a Martin Luther King parade in Las Vegas on Monday, January 15.This video captured by KTNV journalist Joe Bartels shows the moment police made attempts to disperse crowds gathering outside Fremont Casino on Fremont Street. One person can be seen sitting on the floor while receiving treatment from paramedics.As many as 23 minors and six adults were arrested after the 4pm brawl, the Las Vegas Review Journal reported. Meanwhile, KTNV reported, that the number of arrests was just eight.The arrests came after about 100 people began fighting in the street, KTNV reported. Thousands of people attend the annual parade as part of remembrance events for Dr Martin Luther King Jr, it was reported. Credit: Joe Bartels/KTNV via Storyful

AdChoices Icon

Muere el astro gospel Edwin Hawkins

Muere el astro del gospel galardonado con el Grammy Edwin Hawkins

Piratas ceden a McCutchen a Gigantes

Los Piratas ceden al jardinero Andrew McCutchen, quien se incorpora a los Gigantes en un canje

AdChoices Icon

El papa se ve presionado para hacer frente a…

El papa Francisco se verá presionado el martes para abordar un escándalo de abusos sexuales por parte de un sacerdote, en su primer día completo en Chile

AdChoices Icon

“Handmaid's Tale” ampliará sus horizontes en 2da…

Una charla con Elisabeth Moss sobre "The Handmaid's Tale", una historia sobre la pérdida de un hijo y una sociedad totalitaria