Para usted

Líderes en la NBA

Líderes en la NBA

Multiple Arrests After Brawl Breaks Out at Martin…

At least eight people were arrested after a brawl broke out following a Martin Luther King parade in Las Vegas on Monday, January 15.This video captured by KTNV journalist Joe Bartels shows the moment police made attempts to disperse crowds gathering outside Fremont Casino on Fremont Street. One person can be seen sitting on the floor while receiving treatment from paramedics.As many as 23 minors and six adults were arrested after the 4pm brawl, the Las Vegas Review Journal reported. Meanwhile, KTNV reported, that the number of arrests was just eight.The arrests came after about 100 people began fighting in the street, KTNV reported. Thousands of people attend the annual parade as part of remembrance events for Dr Martin Luther King Jr, it was reported. Credit: Joe Bartels/KTNV via Storyful

AdChoices Icon

Muere el astro gospel Edwin Hawkins

Muere el astro del gospel galardonado con el Grammy Edwin Hawkins

Piratas ceden a McCutchen a Gigantes

Los Piratas ceden al jardinero Andrew McCutchen, quien se incorpora a los Gigantes en un canje

AdChoices Icon

Jalisco gana y se mantiene en la Liga Mexicana del Pacífico

Los Charros de Jalisco ganan 2-0 a los Mayos con Navojoa y se mantienen en la serie por un pase a la final en México

AdChoices Icon

“Handmaid's Tale” ampliará sus horizontes en 2da…

Una charla con Elisabeth Moss sobre "The Handmaid's Tale", una historia sobre la pérdida de un hijo y una sociedad totalitaria